AXIS#.CANOPEN​.FC#.FEED

Description

This keyword provides the feed for the additional feedback feed constant calculation. It is part of the scaling calculation used for CANopen object 60E4h, 68E4h Additional position actual value - AxisX.

Context

See CANopen Scaling.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 4294967295

Default Value

65536 (2^16)

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

CAN bus and EtherCAT

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.CANOPEN.FC1.FEED

60e9h

01h

Unsigned32

-

-

Read/Write

No

AXIS1.CANOPEN.FC2.FEED

60e9h

02h

Unsigned32

-

-

Read/Write

No