AXIS#.ECAT​.REPORTWARNINGS

Description

This parameter enables the sending of emergency messages (EMCY) on occurring drive’s warnings via EtherCat.

Value Description
0 Off - No Emergency messages are sent on warnings.
1 Emergency messages will be sent also on drive's warnings

Versions

Action Version Notes
Implemented 02-06-02-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

EtherCAT drives: AKD2G-SPE

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.ECAT.REPORTWARNINGS

501dh

01h

Unsigned8

-

-

Read/Write

No