AXIS#.EIP.STREAMING
Description
This parameter retrieves the current streaming state of the drive for the CIP Sync connection. The parameter's value is set to 1 if the drive is currently accepting and acting upon position set-points from the fieldbus master. Otherwise, the value is set to 0.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-11-00-001 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
7544 |
1 |
7544 (0x1d78) |
AXIS1.EIP.STREAMING |
Unsigned8 |
Read Only |
Yes |
|
73080 |
2 |
7544 (0x1d78) |
AXIS2.EIP.STREAMING |
Unsigned8 |
Read Only |
Yes |