AXIS#.FBUS.IL.CMD

Description

This command allows reading the current command set by the fieldbus when in certain fieldbus modes.

Fieldbus Applicable Modes
EtherCAT Profile torque
CAN Profile torque
PROFINET Torque command written by AXIS#.IL.CMD signal
EtherNet/IP Torque command when using command type 5 (torque) while AXIS#.OPMODE is torque

  • This command can only be written while enabled and reset when the drive changes operation modes. The commanded value is only in affect when AXIS#.CMDSOURCE is set to fieldbus.

Versions

Action Version Notes
Implemented 02-04-06-000

 

General Information

Type

Read/Write

Units

Arms

Range

Minimum range value = maximum of AXIS#.IL.LIMITN and -AXIS#.MOTOR.IPEAK

Maximum range value = minimum of AXIS#.IL.LIMITP and AXIS#.MOTOR.IPEAK

Default Value

0 Arms

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5104

1

5104 (0x13f0)

AXIS1.FBUS.IL.CMD

Signed32

Read/Write

Yes

70640

2

5104 (0x13f0)

AXIS2.FBUS.IL.CMD

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.FBUS.IL.CMD

5104

Float

Read/Write

-