AXIS#.FBUS.BLOCKING

Description

The AXIS#.FBUS.BLOCKING command returns the actual protection state if AXIS#.FBUS.PROTECTION is set.

Value Description
0 Commands are not blocked for “service channel” access.
1 Certain commands are blocked and can not be accessed by “service channel” because the fieldbus master has control.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

AXIS#.FBUS.PROTECTION

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.FBUS.BLOCKING

5005h

02h

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5103

1

5103 (0x13ef)

AXIS1.FBUS.BLOCKING

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.FBUS.BLOCKING

5103

Unsigned8

Read Only

-