AXIS#.HOME.DIST

Description

After the axis has completed the sequence to find the home position, AXIS#.HOME.DIST allows an additional movement, relative to the new home position. This extra movement allows the axis to move away from the found home position by this distance. A value of 0 will prevent any movement and leave the axis at the found home position.

This additional movement uses the homing acceleration, deceleration, and velocity.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Depends on AXIS#.UNIT.PROTARY or AXIS#.UNIT.ACCLINEAR

Rotary: counts, rad, deg, Custom Units, 16-bit counts

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

See Also

AXIS#.HOME.ACC, AXIS#.HOME.DEC, AXIS#.HOME.V

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.DIST

5008h

09h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6104

1

6104 (0x17d8)

AXIS1.HOME.DIST

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.DIST

6104

Signed32

Read/Write

Position

Related Topics

Homing