AXIS#.HOME.MULTITURNMODE

AXIS#.HOME.MULTITURNMODE configures whether Home Found and Home Done (bits 1 and 2 ofAXIS#.MOTIONSTAT) persist when the drive is powered off. This parameter is only used when a multiturn feedback device is configured for AXIS#.PL.FBSOURCE. Positioning moves are only allowed when Home Found and Home Done are set.

Value Description
0

Home Found and Home Done are only set if homing has been completed and neitherDRV.RSTVAR nor AXIS#.HOME.CLEAR has been executed since homing. The home state persists when the drive is powered off and on.

1 Home Found and Home Done are always set.

Versions

Action Version
Implemented 02-01-05-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also AXIS#.MOTIONSTAT
Stored in Non-Volatile Memory Yes

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.MULTITURNMODE

5008h

0dh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6115

1

6115 (0x17e3)

AXIS1.HOME.MULTITURNMODE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.MULTITURNMODE

6115

Unsigned8

Read/Write

-