AXIS#.HOME.OFFSETUSERLIMIT

Description

This keyword limits the range of AXIS#.HOME.OFFSETUSER.

If AXIS#.HOME.OFFSETUSERLIMIT is set to a value smaller than the current value of AXIS#.HOME.OFFSETUSER, that keyword will be reduced to the new limit of AXIS#.HOME.OFFSETUSERLIMIT.

Versions

Action Version Notes
Implemented 02-11-04-000  

General Information

Type Read/Write
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value

N/A

Data Type Float
See Also AXIS#.HOME.OFFSETUSER

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.OFFSETUSERLIMIT

5008h

12h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6121

1

6121 (0x17e9)

AXIS1.HOME.OFFSETUSERLIMIT

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.OFFSETUSERLIMIT

6121

Signed32

Read/Write

Position