AXIS#.HOME.P

Description

AXIS#.HOME.P is the position given to the home point once it is found.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

See Also

AXIS#.HOME.MODE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.P

5008h

0fh

Signed32

Position

-

Read/Write

No

AXIS1.HOME.P

607ch

00h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6109

1

6109 (0x17dd)

AXIS1.HOME.P

Signed32

Read/Write

Yes

71645

2

6109 (0x17dd)

AXIS2.HOME.P

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.P

6109

Signed32

Read/Write

Position

Related Topics

Homing