AXIS#.HOME.PERRTHRESH

Description

AXIS#.HOME.PERRTHRES is the maximum value the absolute following error (AXIS#.PL.ERR ) needs to exceed to detect a mechanical stop.

AXIS#.HOME.PERRTHRES is only used when homing against a mechanical stop using AXIS#.HOME.MODE is 8, 9 or 10.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

180 deg

Data Type

Float

See Also

AXIS#.HOME.IPEAK

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.PERRTHRESH

5008h

06h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6110

1

6110 (0x17de)

AXIS1.HOME.PERRTHRESH

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.PERRTHRESH

6110

Signed32

Read/Write

Position

Related Topics

Homing