AXIS#.HOME.SINGLETURNMODE

AXIS#.HOME.SINGLETURNMODE configures whether Home Found and Home Done (bits 1 and 2 ofAXIS#.MOTIONSTAT) persist when the drive is powered off. This parameter is only used when a singleturn feedback device is configured forAXIS#.PL.FBSOURCE. Positioning moves are only allowed when Home Found and Home Done are set.

Value Description
0 Home Found and Home Done will be clear on reboot.
1

Home Found and Home Done are only set if homing has been completed and neitherDRV.RSTVAR norAXIS#.HOME.CLEAR has been executed since homing. The home state persists when the drive is powered off and on.

Versions

Action Version
Implemented 02-10-03-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also AXIS#.MOTIONSTAT
Stored in Non-Volatile Memory Yes

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.SINGLETURNMODE

5008h

11h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6120

1

6120 (0x17e8)

AXIS1.HOME.SINGLETURNMODE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.SINGLETURNMODE

6120

Unsigned8

Read/Write

-