AXIS#.IL.COGCOMP.MOVETOSTART.V

Description

Sets the velocity used when moving the axis to the Teach Start Position (AXIS#.IL.COGCOMP​.TEACH.POSSTART).

Versions

Action Version Notes
Implemented 02-08-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value 1 rpm

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COGCOMP.MOVETOSTART.V

500ah

26h

Unsigned32

Velocity

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5862

1

5862 (0x16e6)

AXIS1.IL.COGCOMP.MOVETOSTART.V

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.COGCOMP.MOVETOSTART.V

5862

Float

Read/Write

Velocity