AXIS#.IL.COGCOMPH.A

Description

AXIS#.IL.COGCOMPH.A can be used to read / write the amplitudes of the cogging compensation sine waves.

For a given position, the compensation is calculated as follows:

Versions

Action Version Notes
Implemented 02-14-02-000  

General Information

Type

Read/Write Array

Units

N/A

Range

-DRV.IPEAK to DRV.IPEAK

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COGCOMPH.A 0

50dbh

01h

Signed32

-

-

Read/Write

No

AXIS1.IL.COGCOMPH.A 1

50dbh

02h

Signed32

-

-

Read/Write

No

AXIS1.IL.COGCOMPH.A 2

50dbh

03h

Signed32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5867

1

5867 (0x16eb)

AXIS1.IL.COGCOMPH.A

Signed32[3]

Read/Write

Yes

71403

2

5867 (0x16eb)

AXIS2.IL.COGCOMPH.A

Signed32[3]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.COGCOMPH.A

5867

Signed32[3]

Read/Write

-