AXIS#.IL.COMPTABLE.MODULO

Description

The cogging compensation/torque compensation table has a built in modulo that can be used independently of the general position feedback modulo. This modulo is performed on the input to the table (assuming the range is from 0 to AXIS#.IL.COMPTABLE.MODULOVALUE ).

This defines whether or not to apply the modulo operation to the input. For Rotary motors it is suggested to leave this feature on.

When AXIS#.PL.FB is equal to AXIS#.IL.COMPTABLE.MAX, the output of the table will be equal to the last table entry.

Example

To disable the modulo behavior of the table for axis 1, the user would enter:

-->AXIS1.IL.COMPTABLE.MODULO 0

Versions

Action Version Notes
Implemented 02-07-03-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1 (Enabled)

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COMPTABLE.MODULO

500ah

1ch

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5841

1

5841 (0x16d1)

AXIS1.IL.COMPTABLE.MODULO

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.COMPTABLE.MODULO

5841

Unsigned8

Read/Write

-