AXIS#.IL.PWMQUIET
Description
0 - Operate at nominal PWM modulation frequency only. The nominal frequency limits power consumption, but results in acoustic noise.
1 - Automatic control of PWM modulation frequency. Operate at maximum frequency, outside the audible range, when allowable, to eliminate acoustic noise.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.PWMQUIET |
500ah |
17h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5828 |
1 |
5828 (0x16c4) |
AXIS1.IL.PWMQUIET |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.IL.PWMQUIET |
5828 |
Unsigned8 |
Read/Write |
- |
Related Topics