AXIS#.IL.RATELIMITU
Description
This parameter sets the rate of rise and decay on AXIS#.IL.CMDU .
It only affects AXIS#.IL.CMDU – all other currents are not rate limited.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Amps/second |
|
Range |
0 to 2,500,000 |
|
Default Value |
2,500,000 |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.RATELIMITU |
6087h |
00h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5873 |
1 |
5873 (0x16f1) |
AXIS1.IL.RATELIMITU |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.IL.RATELIMITU |
5873 |
Float |
Read/Write |
- |
Related Topics