AXISx.IL.SETCMD

Description

AXIS#.IL.SETCMD applies the AXISx.IL.IUCMDU and AXISx.IL.IVCMDU phase current commands. It performs range checks, applies limits, ensures the axis is in the correct state for using phase currents, and generates the current output.

AXISx.IL.SETCMD is in use when AXIS#.OPMODE = 0 (Torque mode) and AXISx.IL.CMDMODE = 1 (Phase Current mode).

Versions

Action Version Notes
Implemented 02-07-03-000  

General Information

Type Command
Units N/A
Range N/A
Default Value N/A
Data Type N/A
See Also AXISx.IL.CMDMODE, AXISx.IL.IUCMDU, AXISx.IL.IVCMDU
Stored in Non-Volatile Memory N/A

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5833

1

5833 (0x16c9)

AXIS1.IL.SETCMD

Unsigned8

Read/Write

No

71369

2

5833 (0x16c9)

AXIS2.IL.SETCMD

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.SETCMD

5833

Unsigned8

Read/Write

-

Related Topics

Current Loop