AXIS#.JOG.ACC

Description

This keyword sets the acceleration ramp for jog moves.

Versions

Action Version Notes
Implemented 02-04-01-000  
Modified 02-14-02-000 Change to default value to make it more gentle and approprite for how Jog is used.

General Information

Type Read/Write
Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2 , (custom units)/s2

See Acceleration Units for details.

Range Depends on units. See Acceleration Units for details.
Default Value

1,000 rpm/s

Depends on units. See Acceleration Units for details.

Data Type Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.JOG.ACC

501bh

01h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6900

1

6900 (0x1af4)

AXIS1.JOG.ACC

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.JOG.ACC

6900

Float

Read/Write

Acceleration