AXIS#.MT.ACC
Description
Specifies motion task acceleration; active in opmode 2 (position) only.
A value of 0 for AXIS#.MT.ACC after a DRV.LOAD command displays an empty (not initialized) motion task.
Examples
Code
Sets the acceleration of motion task 0 to 1000. The first parameter is the motion task number and the second is the acceleration rate.
-->AXIS1.MT.ACC 0 1000
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write Array |
|
Units |
Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2 See Acceleration Units for details. |
|
Range |
Depends on units. See Acceleration Units for details. |
|
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Commands
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MT.ACC 0 |
50d4h |
01h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 1 |
50d4h |
02h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 2 |
50d4h |
03h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 3 |
50d4h |
04h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 4 |
50d4h |
05h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 5 |
50d4h |
06h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 6 |
50d4h |
07h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 7 |
50d4h |
08h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 8 |
50d4h |
09h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 9 |
50d4h |
0ah |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 10 |
50d4h |
0bh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 11 |
50d4h |
0ch |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 12 |
50d4h |
0dh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 13 |
50d4h |
0eh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 14 |
50d4h |
0fh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 15 |
50d4h |
10h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 16 |
50d4h |
11h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 17 |
50d4h |
12h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 18 |
50d4h |
13h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 19 |
50d4h |
14h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 20 |
50d4h |
15h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 21 |
50d4h |
16h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 22 |
50d4h |
17h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 23 |
50d4h |
18h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 24 |
50d4h |
19h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 25 |
50d4h |
1ah |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 26 |
50d4h |
1bh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 27 |
50d4h |
1ch |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 28 |
50d4h |
1dh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 29 |
50d4h |
1eh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 30 |
50d4h |
1fh |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
AXIS1.MT.ACC 31 |
50d4h |
20h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6300 |
1 |
6300 (0x189c) |
AXIS1.MT.ACC |
Unsigned32[32] |
Read/Write |
Yes |
|
71836 |
2 |
6300 (0x189c) |
AXIS2.MT.ACC |
Unsigned32[32] |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.MT.ACC |
6300 |
Float[32] |
Read/Write |
Acceleration |