AXIS#.MT.MTNEXT

Description

AXIS#.MT.MTNEXT selects which motion task will start when this motion task has completed.

Value Description
<any valid motion task number> The motion task number to start when this motion task completes
–1 There is no next task

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL

Code

MT.MTNEXT 0 1  Will configure Motion Task 0s next task as Motion Task 1.
MT.MTNEXT 0 -1  Will configure no task following Motion Task 0.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read/Write Array
Units N/A
Range -1 to 31
Default Value -1
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

Supported on all drives.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.MTNEXT 0

50d8h

01h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 1

50d8h

02h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 2

50d8h

03h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 3

50d8h

04h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 4

50d8h

05h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 5

50d8h

06h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 6

50d8h

07h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 7

50d8h

08h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 8

50d8h

09h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 9

50d8h

0ah

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 10

50d8h

0bh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 11

50d8h

0ch

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 12

50d8h

0dh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 13

50d8h

0eh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 14

50d8h

0fh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 15

50d8h

10h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 16

50d8h

11h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 17

50d8h

12h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 18

50d8h

13h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 19

50d8h

14h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 20

50d8h

15h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 21

50d8h

16h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 22

50d8h

17h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 23

50d8h

18h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 24

50d8h

19h

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 25

50d8h

1ah

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 26

50d8h

1bh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 27

50d8h

1ch

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 28

50d8h

1dh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 29

50d8h

1eh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 30

50d8h

1fh

Signed8

-

-

Read/Write

No

AXIS1.MT.MTNEXT 31

50d8h

20h

Signed8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6306

1

6306 (0x18a2)

AXIS1.MT.MTNEXT

Signed8[32]

Read/Write

Yes

71842

2

6306 (0x18a2)

AXIS2.MT.MTNEXT

Signed8[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.MTNEXT

6306

Signed8[32]

Read/Write

-