AXIS#.MT.P
Description
Specifies the motion task position. Depending on the motion task control word (AXIS#.MT.CNTL), the AXIS#.MT.P command can either be the target position of the motion task or a relative distance.
Examples
Code
Sets the position of motion task 0 to 360 degrees. The first parameter is the motion task number and the second is the position.
-->AXIS1.MT.P 0 360
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only Array |
|
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
|
Range |
Depends on units. See Position Range for details. |
|
Default Value |
0 |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MT.P 0 |
50d6h |
01h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 1 |
50d6h |
02h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 2 |
50d6h |
03h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 3 |
50d6h |
04h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 4 |
50d6h |
05h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 5 |
50d6h |
06h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 6 |
50d6h |
07h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 7 |
50d6h |
08h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 8 |
50d6h |
09h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 9 |
50d6h |
0ah |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 10 |
50d6h |
0bh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 11 |
50d6h |
0ch |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 12 |
50d6h |
0dh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 13 |
50d6h |
0eh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 14 |
50d6h |
0fh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 15 |
50d6h |
10h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 16 |
50d6h |
11h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 17 |
50d6h |
12h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 18 |
50d6h |
13h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 19 |
50d6h |
14h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 20 |
50d6h |
15h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 21 |
50d6h |
16h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 22 |
50d6h |
17h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 23 |
50d6h |
18h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 24 |
50d6h |
19h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 25 |
50d6h |
1ah |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 26 |
50d6h |
1bh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 27 |
50d6h |
1ch |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 28 |
50d6h |
1dh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 29 |
50d6h |
1eh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 30 |
50d6h |
1fh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.MT.P 31 |
50d6h |
20h |
Signed32 |
Position |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6307 |
1 |
6307 (0x18a3) |
AXIS1.MT.P |
Signed32[32] |
Read/Write |
Yes |
|
71843 |
2 |
6307 (0x18a3) |
AXIS2.MT.P |
Signed32[32] |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.MT.P |
6307 |
Signed32[32] |
Read/Write |
Position |
Related Topics