AXIS#.MT.VCMD

Description

AXIS#.MT.VCMD returns the derivative of the position loop trajectory (AXIS#.PL.CMD) which is a velocity. AXIS#.MT.VCMD is updated while the drive is in AXIS#.OPMODE 2 and processes the following motion types:

  • Motion tasking
  • Homing
  • Electronic gearing
  • Service motion
  • External trajectory coming from a fieldbus
  • External trajectory calculated from an analog input signal

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

Depends on units. See Velocity Units for details.

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.VCMD

50d0h

05h

Signed32

Velocity

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6310

1

6310 (0x18a6)

AXIS1.MT.VCMD

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.VCMD

6310

Float

Read Only

Velocity

Related Topics

Motion Tasks