AXIS#.PL.CMD.MWOFFSET

Description

Position MechaWare (MW) offset is a MW block which adds position to Position command and is designed to interact with MW user models.

Versions

Action Version Notes
Implemented 02-05-05-000

 

Revised 02-08-02-000 Renamed from AXISx.PL.MWFF

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units.

Range

Depends on units. See Position Range.

Default Value

0

Data Type

Float

See Also AXIS#.IL.MWFF, AXIS#.VL.MWFF

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.CMD.MWOFFSET

500ch

16h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5921

1

5921 (0x1721)

AXIS1.PL.CMD.MWOFFSET

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PL.CMD.MWOFFSET

5921

Signed32

Read/Write

Position