AXIS#.PROFINET.FEEDRATIO.SHAFTREV
Description
The count of driving shaft revolutions for the position feed ratio calculation used for PROFINET position units.
See Units.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-02-000 |
General Information
| Type | Read/Write |
| Units |
N/A |
| Range | 1 to 4294967295 |
| Default Value | 1 |
| Data Type | Integer |
| Stored in Non Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP