AXIS#.PROFINET.MAXSOLFAIL

Description

The maximum number of times the sign of life value can be incorrect before faulting. This is used when IRT is active on the PROFINET network to ensure synchronization is maintained.

When set to 65535 the sign-of-life fault detection is disabled.

See Controlword/Statusword 2 and Sign of Life (STW2/ZSW2).

Versions

Action Version Notes
Implemented 02-04-02-000  

General Information

Type Read/Write
Units

N/A

Range 0-65535
Default Value 1
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP

Industrial Ethernet Information

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PROFINET.MAXSOLFAIL

925

Unsigned16

Read/Write

-