AXIS#.PROFINET.xSETPOINTMAP
Description
This command specifies which signals are currently mapped to the setpoints in the axis’ supplemental telegram x. Only signals available in AXIS#.PROFINET.SIGNALLIST labeled as setpoints are allowed to be set. For more information, see Telegram Configuration and Telegram Mappings.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-06-000 |
General Information
| Type | Read/Write |
| Units |
N/A |
| Range | 0 to 65535 |
| Default Value | 0 - Unmapped |
| Data Type | Integer |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP
Industrial Ethernet Information
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.PROFINET.970SETPOINTMAP |
5213 |
Unsigned16[2] |
Read/Write |
- |
|
AXIS1.PROFINET.971SETPOINTMAP |
5215 |
Unsigned16[2] |
Read/Write |
- |
|
AXIS1.PROFINET.972SETPOINTMAP |
5217 |
Unsigned16[2] |
Read/Write |
- |
|
AXIS1.PROFINET.973SETPOINTMAP |
5219 |
Unsigned16[8] |
Read/Write |
- |