AXIS#.UNIT.PIN

Description

AXIS#.UNIT.PIN is used in conjunction with AXIS#.UNIT.POUT to set application specific units. This parameter is used as follows in the drive unit conversion:

  • For position, this parameter sets the units as Custom Units/revolution.
  • For velocity, this parameter sets the units as Custom Units/second.
  • For acceleration/deceleration, this parameter sets the units as Custom Units/second2.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

User units

Range

1 to 4,294,967,295

Default Value

100

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.UNIT.PIN

5010h

01h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6602

1

6602 (0x19ca)

AXIS1.UNIT.PIN

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.UNIT.PIN

6602

Unsigned32

Read/Write

-