AXISx.VL.GEARRATIO
Description
AXISx.VL.GEARRATIO sets the gain between the position loop compensation (AXIS#.PL.KP and AXIS#.PL.KI ) and the velocity loop. In most applications this value should be equal to 1.0. This gain is most important when using a dual loop configuration when there is a disparity between the position loop scaling and velocity loop scaling. These gains are needed to scale the loops to achieve optimal performance.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-14-03-000 | — |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 65536.0 |
|
Default Value |
1.0 |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.