AXIS#.WS.DISARM

Description

This command disables wake and shake immediately. Feedback type is not relevant for this command. If AXIS#.WS.ARM has been issued, the request to execute the wake and shake algorithm at the next enable is cancelled. AXIS#.WS.STATE is set to IDLE.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.DISARM

5013h

14h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6712

1

6712 (0x1a38)

AXIS1.WS.DISARM

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.WS.DISARM

6712

Unsigned8

Read/Write

-

Related Topics

Wake and Shake Overview