AXIS#.DBILIMITACTUAL

Description

This parameter returns the minimum value of the following parameters: AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT.

Example

Assume AXIS1.ICONT = 3 Arms, AXIS1.DBILIMIT = 1 Arms, and AXIS1.MOTOR.ICONT = 2 Arms. Then AXIS#.DBILIMITACTUAL will return 1 Arms.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type

Read only

Description

Returns the minimum value of the AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT keywords.

Units

Arms

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.DBILIMITACTUAL

5000h

11h

Unsigned32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5035

1

5035 (0x13ab)

AXIS1.DBILIMITACTUAL

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.DBILIMITACTUAL

5035

Float

Read Only

-