AXIS#.NAME

Description

This parameter is used to set the name of the axis.

Code

-->AXIS1.NAME Axis 1
-->AXIS2.NAME Axis 2
-->AXIS1.NAME
Axis 1
-->AXIS2.NAME
Axis 2

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

N/A

Default Value

Axis1 for AXIS1 and Axis 2 for AXIS2

Data Type

String

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.NAME

5000h

01h

String(32)

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5000

1

5000 (0x1388)

AXIS1.NAME

String

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.NAME

5000

String

Read/Write

-