AXIS#.TEMPFTHRESH

Description

This parameter returns the over temperature fault threshold of the power circuit for the specified axis. The value depends on the drive model. It is programmed in the drive and cannot be changed.

General Information

Type

Read Only

Units

degC

Range

N/A

Default Value

N/A

Data Type

Float

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TEMPFTHRESH

5000h

14h

Signed32

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5027

1

5027 (0x13a3)

AXIS1.TEMPFTHRESH

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.TEMPFTHRESH

5027

Float

Read Only

-