AXIS#.ZEROREACHED

Description

This keyword indicates if the motor is at zero velocity as configured by AXIS#.ZEROV and AXIS#.ZEROT.

If the absolute filtered velocity (AXIS#.VL.FBFILTER) goes below AXIS#.ZEROV, and the absolute acceleration goes below (AXIS#.ZEROV/AXIS#.ZEROT), for at least AXIS#.ZEROT, then AXIS#.ZEROREACHED is set to 1.

Versions

Action Version Notes
Implemented 02-00-00-000

 

Renamed from AXIS#.ISSETTLED 02-03-00-000  

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.ZEROREACHED

5000h

13h

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5032

1

5032 (0x13a8)

AXIS1.ZEROREACHED

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.ZEROREACHED

5032

Unsigned8

Read Only

-