CAP#.ARM
Description
Arms or disarms the capture channel.
The capture channel needs to be armed to start the process of monitoring the trigger input and sampling the source on the selected edge. Setting CAP#.ARM to zero will stop the capture process.
After each capture event, CAP#.ARM is reset to 0 and must be armed again by setting CAP#.ARM to 1, before another value can be captured. If CAP#.REARM is 1 or 2 then CAP#.ARM stays at 1 and keeps capturing new values until CAP#.ARM is set to zero.
Examples
Usage
0: Disabled (default)
1: Armed
Code
-->CAP1.ARM 1 -->
Context
See Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range |
0 to 1 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | CAP#.REARM |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
CAP1.ARM |
4400h |
09h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
CAP2.ARM |
4401h |
09h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
31000 |
1 |
31000 (0x7918) |
CAP1.ARM |
Unsigned8 |
Read/Write |
Yes |
|
31001 |
1 |
31001 (0x7919) |
CAP2.ARM |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CAP1.ARM |
31000 |
Unsigned8 |
Read/Write |
- |
|
CAP2.ARM |
31001 |
Unsigned8 |
Read/Write |
- |