CAP#.COUNT
Description
The number of capture events that have happened since the drive powered up. If capture is configured to auto-rearm, CAP#.REARM is 1, this counter allows you to detect if a capture event has happened.
Examples
Code
-->CAP1.COUNT 0 -->
Context
See Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range |
N/A |
| Default Value | 0 |
| Data Type | Integer |
| See Also | CAP#.REARM, CAP#.STATE |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
CAP1.COUNT |
4400h |
0ah |
Unsigned16 |
- |
- |
Read only |
No |
|
CAP2.COUNT |
4401h |
0ah |
Unsigned16 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
31010 |
1 |
31010 (0x7922) |
CAP1.COUNT |
Unsigned16 |
Read Only |
Yes |
|
31011 |
1 |
31011 (0x7923) |
CAP2.COUNT |
Unsigned16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CAP1.COUNT |
31010 |
Unsigned16 |
Read Only |
- |
|
CAP2.COUNT |
31011 |
Unsigned16 |
Read Only |
- |