CAP#.T
Description
This will return the captured local clock time. This value is always captured in addition to the position selected by CAP#.SOURCE. The drive local time is the time since boot is in nanoseconds.
Examples
Code
-->CAP1.T 0 [ns] -->
Context
See Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | nanoseconds |
| Range |
N/A |
| Default Value | N/A |
| Data Type | Unsigned64 |
| See Also | CAP#.SOURCE, CAP#.P |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.