DIO#.DIR

Description

Sets or whether the bi-directional IO is an input or output.

Value Description
0 The bi-directional IO is treated as an input signal
1 The bi-directional IO is treated as an output signal

Examples

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0 (input)
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

(missing or bad snippet)