DRV.CUSTOMIDENTIFIER
Description
Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:
- ASCII characters only
- 32 character max length
- No spaces in string
The string is displayed on the device overview screen and in the start page's device discovery table.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
- |
|
Data Type |
String |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DRV.CUSTOMIDENTIFIER |
3000h |
02h |
String(32) |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2010 |
1 |
2010 (0x7da) |
DRV.CUSTOMIDENTIFIER |
String |
Read/Write |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DRV.CUSTOMIDENTIFIER |
2010 |
String |
Read/Write |
- |