DRV.NAME
Description
This parameter is used to set the name of the drive. The assigned name is one way to identify the drive on a network such as a TCP/IP network on which multiple drives reside. The name is restricted as follows:
- Only use ASCII characters
- Max length 32 characters
- No spaces in name
Examples
Usage
Issuing DRV.NAME from the terminal with no value will return the name of the drive.
Code
-->DRV.NAME My_AKD2G
-->DRV.NAME
My_AKD2G
-->
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
no_name |
|
Data Type |
String |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DRV.NAME |
3000h |
01h |
String(30) |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2011 |
1 |
2011 (0x7db) |
DRV.NAME |
String |
Read/Write |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DRV.NAME |
2011 |
String |
Read/Write |
- |