FBUS.DOUT.STATES
Description
This command allows reading the digital output states set by the fieldbus. Each bit corresponds to the state of one digital output (Bit 0 = DOUT1 ... Bit 8 = DOUT9). This is used as the actual digital output state if DOUT#.SOURCE is set to 2 (Fieldbus).
-
- Writing to this command is possible but is not the intended use. When not using the fieldbus, set the digital output values by using DOUT#.SOURCE 0 (User) and set DOUT#.STATEU to the desired digital output state.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-06-000 |
|
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 511 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
No |
Variants Supported
Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
FBUS.DOUT.STATES |
3601h |
01h |
Unsigned32 |
- |
- |
Read/Write |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2703 |
1 |
2703 (0xa8f) |
FBUS.DOUT.STATES |
Unsigned32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FBUS.DOUT.STATES |
2703 |
Unsigned32 |
Read/Write |
- |