FB#.FBUSP

Description

This parameter is the value of FB#.P with a direction applied from FB#.FBUSDIR. It is used by fieldbuses to supply an external feedback value separate from an axis that can be used by the PLC.

Versions

Action Version Notes
Implemented 02-08-02-000

General Information

Type Read Only
Units Counts
Range N/A
Default Value N/A
Data Type Float
Stored in Non-Volatile Memory No

Variants Supported

AKD2G-SPI (EtherNet/IP)
AKD2G-SPP (PROFINET)

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30680

1

30680 (0x77d8)

FB1.FBUSP

Signed32

Read Only

Yes

30681

1

30681 (0x77d9)

FB2.FBUSP

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.FBUSP

30680

Signed32

Read Only

Position

FB2.FBUSP

30681

Signed32

Read Only

Position