FB#.MECHPOS

Description

FB#.MECHPOS reads the mechanical angle which is equal to the lower 32 bits in the 64-bit position feedback word.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

counts

Range

0 to 4,294,967,295 counts

Default Value

N/A

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.MECHPOS

3500h

24h

Unsigned32

-

-

Read only

No

FB2.MECHPOS

3501h

24h

Unsigned32

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30220

1

30220 (0x760c)

FB1.MECHPOS

Unsigned32

Read Only

Yes

30221

1

30221 (0x760d)

FB2.MECHPOS

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.MECHPOS

30220

Unsigned32

Read Only

-

FB2.MECHPOS

30221

Unsigned32

Read Only

-