FB#.POSLOWPASS

Description

FB#.POSLOWPASS configures an averaging filter that is run inside the feedback device at a high data rate. This is used to lower measured position noise and help prevent aliasing from the feedback sampling rate to the drive.

 


  • Currently only SFD-M supports this feature. FB#.POSLOWPASS is only implemented when FB#.SELECT = 47 (SFD-M). It is ignored for other values of FB#.SELECT.

The following table lists the supported filter values.

Value

Notes

0

 No Filter

1

 4 kHz low-pass filter

2

8 kHz low-pass filter

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-14-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.POSLOWPASS

3500h

21h

Unsigned8

-

-

Read/Write

No

FB2.POSLOWPASS

3501h

21h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30880

1

30880 (0x78a0)

FB1.POSLOWPASS

Unsigned8

Read/Write

Yes

30881

1

30881 (0x78a1)

FB2.POSLOWPASS

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.POSLOWPASS

30880

Unsigned8

Read/Write

-

FB2.POSLOWPASS

30881

Unsigned8

Read/Write

-

Related Topics

Scaled Feedback