MW.CONFIGWEN
Description
This parameter enables the MechaWare configuration warning W3101. On first reboot after downloading a new MechaWare user model, W3101 will be enabled regardless of the value of MW.CONFIGWEN.
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-13-01-000 |
- |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 – disabled, 1 - enabled |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
MW.CONFIGWEN |
30e4h |
00h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2860 |
1 |
2860 (0xb2c) |
MW.CONFIGWEN |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
MW.CONFIGWEN |
2860 |
Unsigned8 |
Read/Write |
- |