MW.USERBUFFER#
Description
MW.USERBUFFER allows the user 32 memory values that the user can interact with over telnet, fieldbus and MechaWare.
These values are often used to allow MechaWare to save values from one sample to another, or to provide a simple user interface and often aids in debugging.
There are 32 memory values and the index range is 0 – 31.
-
- The user buffer values can be used for anything but will never have units associated with them, and will always be double precision value.
Example
Set Value
-->MW.USERBUFFER 10 12.3
Read Value
-->MW.USERBUFFER 10
12.300000
Versions
|
Action |
Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | -9223372036854775808.0 to 9223372036854775808.0 |
| Default Value | 0 |
| Data Type | Double |
| Stored in Non-Volatile Memory | Yes |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
MW.USERBUFFER 0 |
30e5h |
01h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 1 |
30e5h |
02h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 2 |
30e5h |
03h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 3 |
30e5h |
04h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 4 |
30e5h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 5 |
30e5h |
06h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 6 |
30e5h |
07h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 7 |
30e5h |
08h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 8 |
30e5h |
09h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 9 |
30e5h |
0ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 10 |
30e5h |
0bh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 11 |
30e5h |
0ch |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 12 |
30e5h |
0dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 13 |
30e5h |
0eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 14 |
30e5h |
0fh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 15 |
30e5h |
10h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 16 |
30e5h |
11h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 17 |
30e5h |
12h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 18 |
30e5h |
13h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 19 |
30e5h |
14h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 20 |
30e5h |
15h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 21 |
30e5h |
16h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 22 |
30e5h |
17h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 23 |
30e5h |
18h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 24 |
30e5h |
19h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 25 |
30e5h |
1ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 26 |
30e5h |
1bh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 27 |
30e5h |
1ch |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 28 |
30e5h |
1dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 29 |
30e5h |
1eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 30 |
30e5h |
1fh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
MW.USERBUFFER 31 |
30e5h |
20h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2800 |
1 |
2800 (0xaf0) |
MW.USERBUFFER |
Signed32[32] |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
MW.USERBUFFER |
2800 |
Float[32] |
Read/Write |
- |