REGEN.TEMP

Description

This parameter returns the measured temperature of the power module for the regen resistor.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read Only

Units

Deg C

Range

N/A

Default Value

N/A

Data Type

Float

See Also

 

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

(missing or bad snippet)