REGEN.TESTSTATUS
Description
Returns the current status of the regen self-test. See REGEN.TEST for more info about the self-test procedure.
|
Name |
Value |
Description |
|---|---|---|
|
Not Started |
0 |
Test has not been started |
|
Running |
1 |
Test is currently running and has not yet failed |
|
Success |
2 |
Test finished successfully |
|
Timed Out |
3 |
Test did not reach setpoint before timeout configured |
|
Short Circuit |
4 |
A short circuit (fault [2013]) was encountered during the test |
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-07-03-000 |
|
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
REGEN.TESTSTATUS |
3007h |
08h |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2407 |
1 |
2407 (0x967) |
REGEN.TESTSTATUS |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.TESTSTATUS |
2407 |
Unsigned8 |
Read Only |
- |