AOI Library, Definitions, & Functionality (CIP Sync)
The section below provides an outline of each CIP Sync AOI's content. A list of Add-On Instructions can be found in Add-On Instructions List.
Format Of Each Entry
- AOI name
- Unconfigured AOI block Default image of what the block looks like and any entries and/or outputs
- Description
- Compatibility
- Expected Command Source and Operation Mode for successful operation
- How the AOI works, its expected behavior, what the AOI is intended for, etc.
- Operands This includes:
- Instance Tag name: Required for every AOI added to the Ladder logic.
- Axis Name: Must be set to the desired axis' unique Axis1 or Axis2 Tag name entered in the CIP_Drive_Comms AOI for the given axis, which points to the AKD2G Module communications for a given IP address.
- Any additional field entries required for the AOI's configuration to be complete and valid.
- Structure This indicates information about the AOI specific to its inputs and outputs.
- Changes to Axis Status bits
- Example of Usage/Programming Guidelines
- Troubleshooting: Summary of Reasons for Errors
- Step Summary
- Revision History