LED and Push-button B1

LED

The Kollmorgen Essentials Drive has an LED on its front side that indicates the status by a tri-color red-green-yellow light.

Color (mouse over icon to animate)

State

Dark

Control board unpowered

Dark, yellow flash

Control board powered, disabled, no faults, warnings

Dark, green flash

Control board powered, disabled, no faults, no warnings

Dimly green

Control board powered but still booting up

Green

Control board powered, enabled, no faults, no warnings

Green/Red blink

Control board powered, downloading in progress

Green, dark flash

Control board powered, dynamic brake active, no faults

Green, yellow flash

Control board powered, enabled, no faults, warnings

Yellow/Red blink (10 seconds)

Control board powered, DRV.BLINKDISPLAY command executed

Red

Control board powered, faults

Dark, red flash Control board powered and running in Recovery mode

 

Push button B1

The Kollmorgen Essentials Drive has a push-button B1 on its top side.

B1 Functions

Description

Recovery Mode Press this button during power up to run in recovery mode.
This mode allows for a firmware file to be downloaded through WorkBench in case the firmware in the servo drive has been corrupted.