Industrial Ethernet Interface Connector X11/X12

The Industrial Ethernet interface has two RJ45 connectors with two associated LEDs at each port.

Industrial Ethernet interface X11/X12 pinout depends on the protocol used. Refer to the matching fieldbus communication manual.

Link/Activity LED

The link/activity LED at each port is green.

LED Meaning
Off no connection
Lit LINK: connection
Flashes activity (packets detected)